Cancel
Showing results for 
Search instead for 
Did you mean: 

ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Valued Contributor
Valued Contributor

Folks.
I filed ER 7695243 with GTAC...Feel free to contact GTAC to add your vote to this ER.

Functionalities requested are not available in NX…but currently available in Hypermill & Mastercam.

 

Hypermill:
• MAXX Roughing & Finishing.
• 5axis helical drilling
• 3D-optimised rest material roughing
• Performance boost for Z-level finishing
• High-performance-cutting (HPC)

 


Mastercam:
• Mastercam Dynamic Milling
• Multiaxis Roughing

 

 

To add your vote via web...go to 

https://webtac.industrysoftware.automation.siemens.com/qtac/index.php5

 

All you need is to enter your company Sold-to and in the "Short Description" :  Add your name to ER 7695243....

 

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP12 | VERICUT 7.3.4
49 REPLIES 49

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Valued Contributor
Valued Contributor
Nice.

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Legend
Legend

Is there a way to add on to this ER without calling in?

 


Dennis Rathi
Creations Unlimited

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Siemens Legend Siemens Legend
Siemens Legend

Hi Kal,

 

I can imagine a couple of reasons to use "5axis helical drilling" but I would like to know when and why YOU would like to setup a "5axis helical drilling" path.

 

Thanks in advance,

 

Toon

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Experimenter
Experimenter

Don't forget

 

Delcam Vortex

Edgecam Waveform - milling and turning

HSM works adaptive clearing

 

All significantly better than any roughing strategy in NX - and volumill

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Legend
Legend

I added to the ER.

 

Feels like throwing a hail mary at the end of a superbowl game... will Siemens catch the ball?

 


Dennis Rathi
Creations Unlimited

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Valued Contributor
Valued Contributor
Once upon a time, the 2012 PLM World CIP Final Rankings had Variable Axis Roughing (module similar to cavity milling, for roughing out multi-axis parts) ranked #3 on the Siemens NX "To Do List"...

Per the ER CAM presentation dated 2012, Variable Axis Roughing would have made it into NX9/NX10...

Forward to April 2016...I am told Variable Axis Roughing is still years(???) away....

Since Siemens has done away with the CIP ER vote rankings, I feel we, the users, are no longer part of the CAM dev. process. Having said that, will the "competitors" functionalities listed in this thread & previous threads (Live B-axis turning, Sandvik Tech Guides machining strategies...etc.) make it into future NX releases...Time will tell...!

So...Yes I agree with you...it is a Hail Mary pass...hopefully to some end zone somewhere & not to some blackhole to never be seen again...but that is up to Siemens...the choice is theirs...machining-machinery technology is constantly evolving...& they need to evolve along and keep up with times!

Hopefully as this ER builds up steam with the support(votes) & backing of all users, Siemens will re-consider & start addressing our machining needs!

Here is the 2012 Rankings:

http://files.plmworld.org/download/3765.3174?AWSAccessKeyId=AKIAJBU23EXMIYKEP2SQ&Expires=1461212233&...


Kal.
CIP= Customer Involvement Process

Previous VAR PLM World CIP Ranking-
#4 Variable Axis Roughing (2007)
#3 Variable Axis Roughing (2008)
#2 Variable Axis Roughing (2009)
#9 Variable Axis Roughing (2010)
#5 Variable Axis Roughing (2011)
#3 Variable Axis Roughing (2012)
NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP12 | VERICUT 7.3.4

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Legend
Legend
Your link to the PLM world file is dead....

Dennis Rathi
Creations Unlimited

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Valued Contributor
Valued Contributor

Crazy...it was working this AMSmiley Sad...Nevertheless...Attached you'll find the 2012 CIP presentation or you might want to use the webcache link below...

 

http://webcache.googleusercontent.com/search?q=cache:65N5ZXjW19oJ:www.plmworld.org/d/do/3174+&cd=4&h...

 

Kal.

NX 9.0.3.4 MP12 | PB 9.0.3.2 | NX11.0.2.7 MP12 | VERICUT 7.3.4

Re: ER 7695243:OPEN MIND Technologies AG (hyperMILL) + Mastercam vs. Siemens NX

Legend
Legend

I submitted on your ER and got the following message back... LOL


*** 21-apr-2016 15:03:25 ****, **** (*****) ***

Hello Dennis,


We only allow one issue per ER. Please fill out the ER template below.

-----------------------------------------------------------------
Please answer the following questions for the Enhancement Request.

What activity in your process is NX not able to currently handle?

What result are you trying to achieve?

Do you currently have a workaround?

Do you have a proposal for the solution you envision NX providing for this capability?

What is the level of productivity gained from such an enhancement?


Dennis Rathi
Creations Unlimited

Learn online





Solution Information