Cancel
Showing results for 
Search instead for 
Did you mean: 

ERROR: The programmed target point is not on the circle path.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi all,

 

I am trying to 'Simulate Machine Code file' but I get this error when the program tries to execute G03.

 

CAM Error.PNGERROR

 

Execution view.PNGExecution View

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

'Simulate machine' works fine.

 

Any help?


Paras Raina, Technical Head, MSC Systems Pvt. Ltd. (India)
NX 12.0.2
Solid Edge 2019
2 REPLIES

Re: ERROR: The programmed target point is not on the circle path.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
1. If your operation with Cutter Compensation - set check box "Use Tool Radius" in Simulation Setting
2. Check your postprocessor output for IJK and G02 G03 settings in MCF - must be a same, for example inc vector from center to start.

Re: ERROR: The programmed target point is not on the circle path.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Generally the CSE driver has a tolerance setting of 0.01 mm for the arc end point error, but yours is 0.4 mm away, so check how the arc is setup as @Chigishev mentioned.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information