Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit "I" address on CSE

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello everybody

 

I’m having a problem with a special machine CSE. I need to edit the I address.

 

image.png

 

This machine is a swiss lathe, with the particularity that X axis is always programed on positive coordinates, regardless if you use the front tools (on the positive side of the X axis) or the rear tools (On the negative side of the X axis). In addition, it is programed on RADIUS coordinates (it’s some common)

Editing the CSE, I got the correct function of the X address (via editing it, as shown)

 

image.png

But I’ve not choice to edit the I address, because it’s on red label.

The only thing I need is to make a smililar edition as I’ve made on X address to I address.

image.png

 

I figure there’s no possible to obtain the “FanucFamily” password in order to copy this one to Current File, so, what other solution you find to invert the sign of the I address only on some tool number???

 

Could someone with access copy to me the internal methacode of the I address, in order to edit it?

 

 

 

1 REPLY

Re: Edit "I" address on CSE

Siemens Phenom Siemens Phenom
Siemens Phenom

I am not sure if the way you do the calculation is the best to go, but if it works fine.

In the "I" command the main CSE command which is used is SetCircleParameter

So that you can try writing your own "I" command with you additions.

 

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information