Cancel
Showing results for 
Search instead for 
Did you mean: 

Engrave on a non flat surface ( project )

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Ant ideas on engraving a surface that is at an angle?  I tried creating an engraving tool path, then optputing the CLS file,  then using surface contour using toolpath as thedrive method, but the retracts are being ignored. 

 

any help would be great

 

Damian

3 REPLIES

Re: Engrave on a non flat surface ( project )

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

i found it............CONTOUR_TEXT

Re: Engrave on a non flat surface ( project )

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Re: Engrave on a non flat surface ( project )


@dforsythe wrote:

i found it............CONTOUR_TEXT


Good to see you found it - this is the answer for drafting or PMI text.

If you are cutting curves from a modeling text feature, you can use surface contouting with Curve/Point drive method. Selection is easier if you set the selection to "Feature Curves".

Mark Rief
Retired Siemens

Learn online





Solution Information