Cancel
Showing results for 
Search instead for 
Did you mean: 

Engrave text

Experimenter
Experimenter

Our designer put planar text on an aluminum plate for me to engrave.  However, I cannot select it to engrave. I'm still pretty new to CAM. I'm out of options.  Please help

4 REPLIES 4

Re: Engrave text

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It depends how they did it.

 

Did they use MODELING text?

Or DRAFTING text?

 

Drafting text can be selected in the various "engrave text" template operations, modeling text can't

 

But you can use modleing text as "drive curves" in various milling operations (set your selection filter to "feature curves" to select all the curves at once, and be able to gracefully handle edits later)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Engrave text

The planar_text and contour_text operations are for drafting and PMI notes only.

 

If the designer made a text feature in modeling, then use fixed_contour, Curve/Point drive method, set the selection intent to feature curves as Ken suggests, and pick the feature. Hopefully the designer used a single stroke font.

 

Mark Rief
Retired Siemens

Re: Engrave text

Experimenter
Experimenter
modeling text. i can't change from note, label, or symbol.

--
Timothy R. Habert Jr
CNC Machining
Anchor Die Technologies, Inc.
4541 Industrial Parkway
Cleveland, Ohio 44135
(216) 671-6000
(216) 671-5369 fax
www.anchor-mfg.com


*Confidentiality Notice:* This email transmission and its attachments, if
any, are confidential and intended only for the use of particular persons
and entities. If you are not the named addressee (or its agent) or this
email has been addressed to you in error, please immediately notify the
sender by reply email and permanently delete the email and its attachments.

--
*Confidentiality Notice:* This email transmission and its attachments, if
any, are confidential and intended only for the use of particular persons
and entities. If you are not the named addressee (or its agent) or this
email has been addressed to you in error, please immediately notify the
sender by reply email and permanently delete the email and its attachments.

Re: Engrave text


@habertt68 wrote:
modeling text. i can't change from note, label, or symbol.


Tim,

Did you try curve/point drive method with feature curves?

Mark Rief
Retired Siemens

Learn online





Solution Information