Cancel
Showing results for 
Search instead for 
Did you mean: 

Engraving Text not Smooth

Experimenter
Experimenter

Almost all the parts manufactured in tool room require some engraving, like the jigs / fixtures need to be identified. Presently in the Planar Text and Contour Text the arcs (eg in O, S...) are segmented instead of smooth arc, this can be seen in the Nx when zoomed. Using this if the manufacturing operation is created the engraving on the CNC machine is also segmented.

Like to know how to overcome this issue.

 

3 REPLIES

Re: Engraving Text not Smooth

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The characters of the NX fonts are created by lines only, there are no arcs at all, so there is nothing you can change.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Engraving Text not Smooth

The NX Fonts are line only, but not the other text fonts.

Try something like Ariel or Calibri and you should see a much smoother path.

Mark Rief
Retired Siemens

Re: Engraving Text not Smooth

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Few years ago it was a same problem for me. Solution - I build my own character font, of course, from lines only, but - with tolerance 0.01 mm.

 

ff

Learn online





Solution Information