Cancel
Showing results for 
Search instead for 
Did you mean: 

Error: Machining Knowledge xml is not a valid Machining Knowledge file

Experimenter
Experimenter

Dear Community,

 

i got a problem with my MKE. Yesterday everything was working properly. I copied the original machine knowledge file to try out some customizations on a safe basis. I taught some features in NX and afterwards had a look at them in the MKE. But now as soon as i teach a feature in NX the file doesn't open anymore in the MKE and shows the attached error message. Where's my fault? On top the advanced file (machine_knowledge_3) is smaller after teaching a feature. (See second picture) How is that possible? I add a new feature recognition and the file becomes smaller? Doesn't make sense for me.

 

Thanks a lot in advance for your efforts!

 

Regards

Carlo

1 REPLY 1

Re: Error: Machining Knowledge xml is not a valid Machining Knowledge file

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Carlo,

 

This is not an typical error; I haven't seen it before. The XML file is probably corrupt; no idea yet what's wrong but I will be happy to take a look if you can send it to me in a private/personal message so that I can try to repair it.

 

I wouldn't worry too much about the size of the XML file.

 

Tom van 't Erve

NX CAM Development

Learn online





Solution Information