Cancel
Showing results for 
Search instead for 
Did you mean: 

Error:"No feed value set. Linear motion will not be executed. "

Genius
Genius

When I was using the sync manager for mill turn simulation, I got the error:"No feed value set. Linear motion will not be executed. "

 

How to fix that error?

 

ThankCapture.PNG

3 REPLIES

Re: Error:"No feed value set. Linear motion will not be executed. "

Siemens Phenom Siemens Phenom
Siemens Phenom

HI SeanHAI

Check that you have a spindle speed as the feedrate could be set to mmpr so no spindle speed results in no linear feedrate.

Regards

Paul

Re: Error:"No feed value set. Linear motion will not be executed. "

Siemens Phenom Siemens Phenom
Siemens Phenom

If that happens when you enter the Synch-Manager WITHOUT any synchronisation marks that could happen by nature as some operations are not correctly synched. e.g. different channels will address the main work piece spindle with G95 G96, that could result in such a message.

 

Hope that helps.

 

2017-05-29 10_24_31-Best Practice MillTurn Demo_V10.0.3 V1.pptx - PowerPoint.png

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Error:"No feed value set. Linear motion will not be executed. "

Genius
Genius

Hello Tom

 

Could you post that whole PPT file, so I can learn more about sync manager in the CAM.

 

Thanks

Learn online





Solution Information