Cancel
Showing results for 
Search instead for 
Did you mean: 

Error with IPW update

Genius
Genius

Hi,

 

I have an IPW update error, I am doing some step wrong. Attached the error photos.IPWerror1.jpg

 

IPWerror2.jpg.

 

Actually I am using NX9.0.2.5

 

Thanks, Igor.

2 REPLIES 2

Re: Error with IPW update

If this is a single part in multiple positions, then the PART geometry in both workpieces must point to the same component, just in different positions. That's my best guess, but we really need more information to help you.

 

There are some tech tips on IPW Flow and paste with reference that may help. Otherwise, give GTAC a call and they can take a look at it.

Mark Rief
Retired Siemens

Re: Error with IPW update

Genius
Genius

Hi Mark,

 

You are right is a single part with different positions.

Learn online





Solution Information