Cancel
Showing results for 
Search instead for 
Did you mean: 

Explore UDE

Pioneer
Pioneer

Hello,

When I input UDE in some of the operation of tool path. I need open the tool path to see UDE. Do we have a way to open the file or other menus to see all of the UDE which was used for this part?

 

Thanks in advance!

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
4 REPLIES 4
Highlighted

Re: Explore UDE

Gears Phenom Gears Phenom
Gears Phenom

"to see all of the UDE which was used" - I think no

- you can add column with start/end events - it tells you if any ude is located on object

-right click on operation (or any object) - object - start/end events

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Explore UDE

Siemens Genius Siemens Genius
Siemens Genius

Hi  Canateda,

 

Juraj is absoluetly right, the most convinient way to get an overview of your UDE is through an additional column in the ONT.

 

How to get it, you can see in this picture:

2017-09-04 14_07_21-NX 11 - Manufacturing - [sim09_turnmill_5ax_cam_sinumerik_mm.prt (Modified) ].png

 

Regards,

Florian Weisse

 

Re: Explore UDE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You might also want to check out this thread:

 

https://community.plm.automation.siemens.com/t5/Discussion-Forum-NX-Manufacturing/List-almost-all-UD...

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Explore UDE

Experimenter
Experimenter
This is the best way as shown above.. also hover mouse pointer over the column in the ONT for a preview of the UDE commands active within. Hope this helps

Malc

Learn online





Solution Information