Cancel
Showing results for 
Search instead for 
Did you mean: 

Export Characteristic data like nominal size and tolerance for the usage in a Q-Program

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi there,

 

does anyone know if it is possible to export the PMI-Information from a component? Like nominal size, tolerance and Feature Contol Frames. From NX CAD or NX CMM Inspection.

Preferably the Q-DAS format.

 

Thanks for your help.

 

Regards,

Michael

4 REPLIES 4

Re: Export Characteristic data like nominal size and tolerance for the usage in a Q-Program

Legend
Legend

Are you asking for in-built NX option, NX custom tool or export using any 3rd party software?

Re: Export Characteristic data like nominal size and tolerance for the usage in a Q-Program

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

BCT Inspector can extract all the PMI, and output it to Excel (or whatever)

Not sure about QDas format, specifically

http://www.bct-technology.com/

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Export Characteristic data like nominal size and tolerance for the usage in a Q-Program

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

thanks for your response.

It should be a NX in-built option. No 3rd party software.

Re: Export Characteristic data like nominal size and tolerance for the usage in a Q-Program

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I know of no built-in option.

You can write your own API program to query a part for all the PMI data & output it as desired.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information