Cancel
Showing results for 
Search instead for 
Did you mean: 

Exporting NX CAM Operations

Experimenter
Experimenter

Is there any way to export the operation list from a prt file?

For example I have a short machining program that I'd want to export to another file, like the one attached.operations.png

The idea behind this is to have an additional file so that I can save multiple NC programs for the same prt file.

 

 

 

3 REPLIES

Re: Exporting NX CAM Operations

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The simplest way is to use Copy/Paste
- Open both files in one NX session

- Copy all operations you want in first file

- Switch to another file
- Paste operations

 

The other way is to use your own template file
You  can find some basics about it here:

https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX-Manufacturing/Getting-st...

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Exporting NX CAM Operations

If you want to export an operation list, use shopdocs or export from the Operation Navigator.

If you want the operations, then copy/paste or browse your part as a template, like @Marek_Pawlus says.

If you want multiple programs for the same part, be sure you are using assemblies, and not creating the operations in the same part as the geometry. If you use file new, you can easily create several setups that reference the same part.

 

Mark Rief
Retired Siemens

Re: Exporting NX CAM Operations

Experimenter
Experimenter

Thank you!

Exactly what I needed

Learn online





Solution Information