Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Extend paths / overlap in floor wall / rest material machining

Phenom
Phenom

Hello,

 

I want to ask about this overlap parameter in floor wall operation.

In planar mill  exists and it is working. (not overlap in non cutting moves in star/drill points)

Snímka.JPG 

 

 

 

 

 

 

 

 

 Bez názvu.jpg

 

 

 

Because I want to machine rest material but not exactly on its start but with little offset.

 

Look at the path and material in floor wall operation:

Snímdka.JPG

If the tool enagages into material in the same place where previous tool ends it leaves mark on the wall.

I want to machine it.

 

See attached part.

Thank you for your answers

 

jb

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
5 REPLIES

Re: Extend paths / overlap in floor wall / rest material machining

Phenom
Phenom

Did anybody notice that?

Snímka.JPG

 

Snímka2.JPG

 

Preview of material is not good and if it be on good position, the cut path is not precisely on the start of the rest material.

Plus I want extend cut path because there will be little amount of the rest material.

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Extend paths / overlap in floor wall / rest material machining

The overlap distance you show in the dialog picture is for reference tool and 2D IPW containment.

You are asking about floor/wall with IPW. Are you looking to control the overlap there?

Mark Rief
Retired Siemens

Re: Extend paths / overlap in floor wall / rest material machining

Phenom
Phenom

Hello, exactly

 

one way to extend the path is using the linear engage and retract as the default setting is.

But it seems to be a "rough" way.

Snímka.JPG

(blue line marks where is the rest material. previous tool was D20, next tool is D10 mm)

 

If you look closely the cut move starts even behind the blue line.

It should start at the the point where blue line is.

And I want to extend it to start cut before the blue line like overlap paramer do in plannar mill with reference tool.

 

jb

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Extend paths / overlap in floor wall / rest material machining

I confirmed that the overlap distance is not a user controlled parameter in floor/wall milling. This would be an enhancement. 

Mark Rief
Retired Siemens

Re: Extend paths / overlap in floor wall / rest material machining

Phenom
Phenom

I think you are right.

If you can push it to the development it would be good.

I hope that it will helps everybody.

 

thank you

 

jb

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information