Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Extra point when mirroring ( at only return and gohome avoidance point )

Pioneer
Pioneer

Hello all, Again,

 

It seems that when I mirror an event (X) and it has in non cutting moves an avoidance return point established.

The mirrored MO has the point proper but an added extra point shows up at the original location (not-mirrored).

This does not happen if I have a start point. Only return and gohome point.

I originally had goto points in the "Machine control" start and end of paths events area. They definatly did not mirror.

This is a 90 deg head drill and these are my starting points at the clearance plane before and after going down to the hole on its tool axis direction. I really do not want to hand edit out these points. There are many.

 

I am wondering if this is a bug.


GOTO/15.487613,-20.140134,-0.700378,0.3195223,-0.9455875,-0.0613987
FEDRAT/IPM,50.000000
GOTO/15.423708,-19.951016,-0.688099
FEDRAT/1.000000
GOTO/15.311815,-19.619881,-0.666597
FEDRAT/50.000000
GOTO/15.503528,-20.187234,-0.703437
GOTO/19.303359,-22.084334,7.000000
RAPID
GOTO/-19.303359,-22.084334,7.000000 <<<<<<<<<<<<<<<<<<

 

The goto point above is the correct goto NX adds the arrowed line all by itself.

 

Oh and I am in 11.0.2.7 MP10

3 REPLIES 3

Re: Extra point when mirroring ( at only return and gohome avoidance point )

Pioneer
Pioneer

ok, found an update of MP11

Updated and still the same.  Smiley Sad

Re: Extra point when mirroring ( at only return and gohome avoidance point )

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This issue is first fixed in NX 12, but I don't know the exact release.

I have had a report of this issue a few weeks ago and was testing with NX 12.0.2 MP3 (latest release NX 12.0.2 MP4).

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Extra point when mirroring ( at only return and gohome avoidance point )

Pioneer
Pioneer

Installed NX12.0 and updated to 12.0.2 MP04

Seems to be fixed.

Learn online





Solution Information