Cancel
Showing results for 
Search instead for 
Did you mean: 

Extract curves from ToolPath

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello all, i want to extract the curves from a toolpath and make it as splines in 3D.

 

It's because i need to trim a surface using as limit the center path of the tool.

 

Tanks!

3 REPLIES

Re: Extract curves from ToolPath

If you are a licensed user, there is info on this in the archives:

 

Attached is a  program that did that with a CLS in GRIP over 20 years ago.

Rename .txt to .grs, compile and link.

If it needs updating, have fun, or contact the author - he is still in GTAC.

Mark Rief
Retired Siemens

Re: Extract curves from ToolPath

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thank you very much Mark, I'll try. (Actually first I'll see how it works and how to run NX)

Anyway, I solved the problem already. I guess what I did is something very similar to this script, but I did it manually.

The steps were:

-Otput the CLS from the ToolPath.

-Edit On a notepad the CLS, deleting the header and each block the word GOTO /
Replace also the comma coordinate separators to spaces.

Being something like this:

-2.4309 -80.8068 65.4000
-2.4309 -80.8068 -3.5440
-2.4309 -80.8068 -48.5000
-3.2371 -80.8068 -48.5000
-3.9614 -80.7706 -48.5000
-4.6857 -80.7301 -48.5000
-6.1343 -80.6236 -48.5000
-6.8585 -80.5619 -48.5000
-7.5828 -80.4937 -48.5000
-8.3071 -80.4235 -48.5000
-9.0314 -80.3447 -48.5000
-9.7557 -80.2574 -48.5000
-11.2042 -80.0629 -48.5000
-11.9285 -79.9585 -48.5000


With this text file ready, I went back to NX and went to:
File> Import> Points from file.

With the points already in 3D, I joined with: Curve> Fit curve



I leave the steps followed, if someone serves them.

Re: Extract curves from ToolPath

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thank you very much Mark, I tried to use that .grs but could not.
However, I could use a Grip rose another user on the link you put, and it works wonders!

Thank you very much, I save a lot of time.

The grip that i used, is "6048_GRIP.zip"

Learn online





Solution Information