Cancel
Showing results for 
Search instead for 
Did you mean: 

FASC - arc output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just migrated from NX7.5 to NX10.0.3.5 MP5.

We have some fixed axis contouring operations on a part.

Part geometry is roughly a cylinder with "blobs" attached (mounting lugs, etc.)

(fixed) Tool axis is perpendicular to cylinder centerline, zig passes cut along the circumference.

Arcs output set to parallel/perpendicular to tool axis.

In NX 7.5, many (not all) passes were mostly arc output (with exceptions around the blobs) ("arc" = internal toolpath CIRCLE/ line)

In NX10, when regenerating these operations, a *few* passes remain as arcs, but many passes turn into "a whole bunch of linear moves".  Users are not happy :-(

I called GTAC, but I never got an email with the IR number.  But other than making the tolerance tighter (which didn't work particularly well - there were a few more arcs, but a LOT more linear moves), they didn't have much to offer.

 

Are there any other things that will trigger this change, or force NX to prefer arcs to linear moves?

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


7 REPLIES

Re: FASC - arc output

Gears Phenom Gears Phenom
Gears Phenom

Make the Intol - Outol looser not tighter.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: FASC - arc output

Are the "roughly" cylindrical surfaces true analytic cylinders? Or just surfaces that approximate a cylinder?

 

Mark Rief
Retired Siemens

Re: FASC - arc output

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Iam 100% agree with KEN_A - something is wrong with mill arc interpolation till last update in NX10 . I remeber nx 8.5 , arcs were fine in any planars (XY , ZX , ZY). My friend notice same issue last 3 days ago on NX10, we compare our work and install new MP pack on nx ( 10.0.3.5 MP8 )  - nothing change - arcs in ZY or ZX do not generate as KEN_A says above , there are too many lines and mayby three or five shredded arcs on whole area, and the surface after finish milling looks like rasper . PRT model came from nx 10 (same environment) and was modeled by using simple cylinder and extrude feature with 798 mm diameter .

 

I attach the picture, everything is shown there

 

As a summary - XY interpolation is working good,

ZX and ZY interpolation is working as lottery , sometimes better sometimes worse.

NX 8.5 did not have this problem.

 

Best regards, Jacob

========================================
Engineering >> NX10.0 Performance in the making

Re: FASC - arc output

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I have enclosed a test model from NX 10 by using contour_area operations.

Look on two operations:

* contour_area_ZX

* contour_area_ZY

 

Yes, arcs are there, but there are also unnecessary lines.

I notice that sometimes setting tolerane are helping but try to set part stock on 0.05 or 0.1  - its much better but its not a solution.

 

I noticed that sometimes all NX Postprocesors (and not only my own) doesnt output arcs on G18 and G19 from contour_area. But when I type part stock from 0 to 0.05 Postprocesor start output arcs.

 

========================================
Engineering >> NX10.0 Performance in the making

Re: FASC - arc output

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I have the same issue as Ken_A with arc interpolate in all planars.

Best regards, Daniel

Re: FASC - arc output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Has anyone already reported this problem?

Was the problem listed as fixed in the release notes of the MR or MP you installed?

 

If Siemens doesn't know about it, there will be no fix in any release.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: FASC - arc output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

PR 7804484

And Mark, yes, they are true cylinders/cones (see example part in the PR) 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information