Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FBM Hole Milling - Depth

Valued Contributor
Valued Contributor

Hello,

 

i would like to set in MKE manually a Depth for my Hole Milling operation.

Is that possible maybe as an Add-on ? I did not find any suitible type.

I need the same also for Spot Drilling - the standard here is 3 mm.

 

Thank you.

NX 11.0.1.11
2 REPLIES

Re: FBM Hole Milling - Depth

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

With NX 11.0.2 you can set the option to use a predefined depth value for hole milling.

In earlier releases you would need a HoleThrough or HoleBlind add-on respectively and set the depth.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: FBM Hole Milling - Depth

Valued Contributor
Valued Contributor

Got it! Thank you Smiley Happy

NX 11.0.1.11

Learn online





Solution Information