Cancel
Showing results for 
Search instead for 
Did you mean: 

FBM for Z Level type and mill planar type operation

Creator
Creator

Hi all,

    It's successful for me to load a hole making type and cavity mill type operation after I grouped the features. But for Z Level type and mill planar type operation I was failed to do that? So what kind of feature should I teach for?

4 REPLIES 4

Re: FBM for Z Level type and mill planar type operation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Oscar,

 

It is not entirely clear to me what you are trying to do.

Are you teaching operation sets ?

Are you trying the ootb machining rules ?

Can you provide a part please and a short description.

Your NX version is important to know too.

 

Reinier Capelle
NX CAM Development - Customer Success

Re: FBM for Z Level type and mill planar type operation

Creator
Creator

Dear Reinier

   Thank you for your reply.

   1.My NX version is 11.0.2.7

   2.1For pic 1 surface contouring operation I can use the geometry which is grouped from the feature that is find.

   2.2For pic 2 Z level profile I can't select the grouped feature.

   3.Sample is attached.

   Thank you once again.

 

 

Re: FBM for Z Level type and mill planar type operation

Creator
Creator

I lost the attachment. Here it is.

Re: FBM for Z Level type and mill planar type operation

Siemens Phenom Siemens Phenom
Siemens Phenom

Z-Level Profile operation needs a MILL_AREA geometry parent.

Reinier Capelle
NX CAM Development - Customer Success

Learn online





Solution Information