Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

FBM hole_making.HOLE_MILLING Axial Stepover Multiple

Valued Contributor
Valued Contributor

Hello there,

 

I am working on the operation of hole_making.HOLE_MILLING in feature based machining. I want to set the Axial Stepover as type "Multiple" in MKE Add-on. For example, I tried to set two values, my code is:

 

as.Axial_Stepover_Variable_Passes = 1
as.Axial_Stepover_Variable_Values = 0.2
as.Axial_Stepover_Variable_Values__Unit = "PartUnits"

as.Axial_Stepover_Variable_Passes = 1
as.Axial_Stepover_Variable_Values = 0.5
as.Axial_Stepover_Variable_Values__Unit = "PartUnits"

 

It always gave me the following error:

Compute Operations Error 65 : Internal error

 

It seems that I can only set one value.

 

Thanks,

Kai

1 REPLY 1

Re: FBM hole_making.HOLE_MILLING Axial Stepover Multiple

Valued Contributor
Valued Contributor

Thanks, I solved it by myself. I added two Add-on's for that.

 

 

Learn online





Solution Information