Cancel
Showing results for 
Search instead for 
Did you mean: 

FLOOR_WALL won't start cutting at blank height.

Pioneer
Pioneer

I have it set up as a WORKPIECE with my blank selected within that.  I am able to leave .100" or any amount I want on the floor but I cannot get the toolpath to start at the blank height.  It seems to want to start from the part height.  I have it set to Blank Geometry in the containment tab.

 

Capture.JPGCapture2.JPGCapture3.JPG 

4 REPLIES 4

Re: FLOOR_WALL won't start cutting at blank height.

Siemens Phenom Siemens Phenom
Siemens Phenom

i was able to get the tool to cut top of part as firts level by changeing my Blank to Thickness, setting to stock + depth of first cut.

ScreenHunter_01 Jun. 26 15.34.gifScreenHunter_02 Jun. 26 15.35.gif

Re: FLOOR_WALL won't start cutting at blank height.

Pioneer
Pioneer

I probably should have mentioned that I already tried this.  The channel is 1.500" deep and the blank is .175" above the part.  Changing the Blank to "Thickness" instead of "Blank Geometry" and entering 1.675" gives me the same thing.

Re: FLOOR_WALL won't start cutting at blank height.

Legend
Legend

For me it works

 27-06-_2018_08-44-12.png

 

Re: FLOOR_WALL won't start cutting at blank height.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not a floor/wall expert, but isn't there a setting to tell f/w whether to take the blank into account, or not?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information