Cancel
Showing results for 
Search instead for 
Did you mean: 

Face Grooving

Valued Contributor
Valued Contributor

Cutting a face groove and spath is generated below center instead of normal position

Mike

NX 11.0.2.7
Win 7
2 REPLIES

Re: Face Grooving

Valued Contributor
Valued Contributor

I found the issue I had tool at a point below center in previous operation, I put in new approach and is fine

Mike

NX 11.0.2.7
Win 7

Re: Face Grooving

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, if there are multiple cut regions, turning will always use the closest one to the last tool position.

 

I typically always add a avoidance turning geometry parent with a from point to minimize this.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information