Cancel
Showing results for 
Search instead for 
Did you mean: 

Face Milling

Valued Contributor
Valued Contributor

Hello

 

I Have a question...

If i create a face milling operation with Zig-Zag toolpath, the toolpath retracts on every cutting depth.

Is there an option to cut backward?

 

Generated path:

 

Now.png

Edited path:

 

Edited.png

Thank you


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}
5 REPLIES 5

Re: Face Milling

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I think - it impossible for facemilling operation. You can use Sequential Milling, not so easy, but..

Re: Face Milling

Valued Contributor
Valued Contributor

Okey thank you.

I asked because the first cam i've used was Mastercam 9.1 and there was a button to set the toolpath after stepdown backword.

The searching for this button has endet Smiley Wink

 


Production: {NX 10.0.3.5 MP18}
Testing: {NX 12.0.2.9 MP03}

Re: Face Milling

Pioneer
Pioneer

How to do this edition?

Highlighted

Re: Face Milling

In the tool path editor, set the selection to cut level, select a level, and reverse it.

Mark Rief
Retired Siemens

Re: Face Milling

Pioneer
Pioneer

I could not do Can you make a video to help me?

Learn online





Solution Information