Cancel
Showing results for 
Search instead for 
Did you mean: 

Face milling NX9 - missing command

Builder
Builder

Hello,

in operation Face milling (NX9) is missing comand "Ignore holes" in  specify face boundaries.

How to simply ignore holes in this operation? In NX8.5 is this option alloved.

Thanks.

3 REPLIES 3

Re: Face milling NX9 - missing command

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Note that default NX9 now ignores the holes.

 

If you whant to avoid some holes:

From what I could see, maybe I'm wrong, what you can do now is add new set, with holes NX you want to avoid .

Re: Face milling NX9 - missing command

Builder
Builder

Ok, option to control holes, island, champfers is on top of screen.

Re: Face milling NX9 - missing command


@gajdos wrote:

Ok, option to control holes, island, champfers is in top of screen.


Glad you found it on the Selection Bar. Many selection options or intent settings that are common to multiple dialogs can be found here.

Mark Rief
Retired Siemens

Learn online





Solution Information