Cancel
Showing results for 
Search instead for 
Did you mean: 

Facet Error with IPW update used Teamcenter

Experimenter
Experimenter

 

Hi,

i will load a "blank" from Teamcenter like this:

 

01.JPG

 

I select it from teamcenter and i Update Local IPW from Source like this:

 

02.JPG03.JPG04.JPG

 

I become an Error :

&MACRO EVENT FOCUS_IN 1 0, 25231360, 0, 0, 0! Update Local IPW from Source
&MACRO EVENT ACTIVATE 1 0, 25231360, 0, 0, 0! <DLC> Update Local IPW from Source
*** EXCEPTION: Error code  3295013 in line 2198 of D:\workdir\Patches\nx903_patch\src\cams\no\ind\dctk.c at Thu Apr 26 08:06:57 2018 Mitteleuropäische Sommerzeit
+++ Facet error
[ 1] 07FEFD4DA06D                                                              (KERNELBASE)

.

.

 

Has anyone an Idea for solution or reason for this problem?

Some Parts it works and some Parts doesnt't work and show an Faceterror.

Greetings

Oliver

 

 

3 REPLIES 3

Re: Facet Error with IPW update used Teamcenter

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Oliver,

 

before I can state more I like to ask you to provide me the entire syslog.

If you not like to share to all you can send it to me directly in the community.

 

Thomas

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Facet Error with IPW update used Teamcenter

Experimenter
Experimenter

Here is the syslog:

 

Greetings.

 

Re: Facet Error with IPW update used Teamcenter

Experimenter
Experimenter

Here is another syslog

 

without the Error.

 

In this part it works fine.

 

Greetings.

Oliver

Learn online





Solution Information