Cancel
Showing results for 
Search instead for 
Did you mean: 

Fanuc Cs Contouring - NX method - post - ISV

Phenom
Phenom

Has anyone tried to implement this? I have a DMG Mori NTX2000 where we would like to do this. I can't find any example of G code in searches or in manuals. Fanuc has not answered my requests for examples yet. Not getting the impression the MTB has much experience programming it. They did provide an example of running helical circles in synced mode - I think this would be terrible for contours (though.) I was hoping that the G code would look like a lathe. Okuma seems to have this implemented that way.

NX12.02
Windows 10 Pro
2 REPLIES
Highlighted

Re: Fanuc Cs Contouring - NX method - post - ISV

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've done the Okuma variant (post only, no IS&V)

Done as a linked lathe post

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Fanuc Cs Contouring - NX method - post - ISV

Phenom
Phenom

Yes - I hope that G code is lathe style. Hard to believe it is so hard to find G code program examples.

NX12.02
Windows 10 Pro

Learn online





Solution Information