Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Based Machining, Axial Stepover, Exact

Valued Contributor
Valued Contributor

Hello there,

 

I am working on the hole_making.HOLE_MILLING operation. I am trying to set the Path Settings -> Axial -> Axial Stepover as "Exact". I find that in the Add-on, I can only set it as other types (Constant, Multiple, Passes, %Flute Length), but cannot find type "Exact". Although type Constant and type Exact sound the same, but they may create different machining paths (Please find the attached example). I have tried teaching this operation, but couldn't find the type either.

 

Regards,

Kai

1 REPLY 1

Re: Feature Based Machining, Axial Stepover, Exact

Siemens Phenom Siemens Phenom
Siemens Phenom

Axial Stepover Type = Exact is not yet supported by Create Feature Process for CylinderMilling. This is a caveat. I created an internal PR to fix this issue.
As a workaround, you can fix this Stepover type in your operation template. Thank you !

Reinier Capelle
NX CAM Development - Customer Success

Learn online





Solution Information