Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Based Machining - Introduction Presentation

Genius
Genius
Hi, Anyone has the introductory presentation slides which explains: 1) What is Feature Based Machining (FBM)? 2) How it works? I am looking for 2 to 4 slides, high level to show to stakeholders who will understand the concept. Appreciate your help !
9 REPLIES

Re: Feature Based Machining - Introduction Presentation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Here is high level introduction presentation.

Let me know if you have any additional questions

 

Tom van 't Erve

NX CAM Development

Re: Feature Based Machining - Introduction Presentation

Genius
Genius
Thanks a lot TomvantErve ! This is what I am looking for in addition to little information I have.

Re: Feature Based Machining - Introduction Presentation

Genius
Genius

Hi,

I am looking for a consultant who will do a FBM pilot for 2 componenets.
Activities are:

1) Define rules/features/criteris/process in Machining Knowledge Editor for features which are in these 2 components (Setup MKE for FMB)
2) Demonstrate FBM on first component
     a) Run feature recognition
     b) Generate NC code
     c) Post Process operations ( PP available with MACH Setup)

3) Run step 1 and 2 on 2nd component from same family of part.

 

Do you know anyone who can do this ? Please respond contact details.

Re: Feature Based Machining - Introduction Presentation

Siemens Legend Siemens Legend
Siemens Legend

Did you try the OOTB features and their machining rules ? For a demo/pilot this will usually be enough. If it needs to be more customized, entry level customization can be done with Teach Operation Sets. Any CAM user can do this. No special skills are required. Teach Operation Sets is available in preview in NX 10.0.3 MP1.

Reinier Capelle
NX CAM Development - Customer Success

Re: Feature Based Machining - Introduction Presentation

Genius
Genius

Hi Reinier Capelle : How easy it is in NX 9.0.3 ?

Re: Feature Based Machining - Introduction Presentation

Siemens Legend Siemens Legend
Siemens Legend
In NX 9.0.3 you can also use the OOTB features and machining rules. FBM is only 2 commands: Find Features and Create Feature Process.
Teach Operation Sets is available in preview in NX 10.0.3 MP1 and not in NX9. However, the machining rules can be imported into an NX 9.0.3 library, using the MKE export/import commands.


Reinier Capelle
NX CAM Development - Customer Success
Highlighted

Re: Feature Based Machining - Introduction Presentation

Genius
Genius
Hi ReinierCapelle, Does it mean I can define Teach Operation in NX 10.0.3 MP1, define machineing rules there and import in NX 9's MKE?

Re: Feature Based Machining - Introduction Presentation

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, that's what Reinier tried to explain.


You can use the (preview) Operation Set Teaching in NX10.0.3 MPx which will create new rule sets; open the XML using the NX10.0.3 MPx Machining Knowledge Editor, export them to an XML file, import the XML file into the NX9.0.x Machining Knowledge Editor and use them in NX9.0.x NX CAM.

 

Tom van 't Erve

NX CAM Development

Re: Feature Based Machining - Introduction Presentation

Experimenter
Experimenter

Hello Mak,

 

With reference to your above requirement, we in TCS have a team working on NX FBM.

Currently we are supporting for one of the major customer for Manufacturing of Subsea components through FBM.

With the vast manufacturing experience along with emerging technology of NX FBM, We are looking forward to support you with the activities you are looking for.

For further discussion feel free to contact me on my official mail ID, mohanbabu.k@tcs.com

 

Looking forward to hear from you,

 

Warm regards,
Mohan

Tata Consultancy Services

Learn online





Solution Information