Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Teaching - Machining Areas

Valued Contributor
Valued Contributor

Hi, 

 

i have teached the MKE a new Feature, know I would like 

to create operations for that feature to teach them the system. 

I have defined all the PMI's and Machining Areas. MACH_1 is the floor MACH_2 i have selected

the Wall.

Now I want to create a Hole making Operation but the Drilling dont go through the hole depth. 

 

Hope you can help me thank you. 

NX 11.0.1.11
2 REPLIES

Re: Feature Teaching - Machining Areas

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried the MACH_1 area instead, which seems to be more like the regular FACES_BOTTOM area of a hole machining feature?

The alert in the bottom corner tells it all, your areas are not as expected for a hole.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Feature Teaching - Machining Areas

Siemens Phenom Siemens Phenom
Siemens Phenom

I did a quick test in NX11.0.1 using your MACH2 machining area and it works fine (you still get the warnings but it works).

 

If you are on an earlier version you may want to try the MODEL_DEPTH machining area (this is always available for a DRILLING operation; you don't need to teach it). This should also give you the correct depth.

 

NX CAM Development

Tom van 't Erve

Learn online





Solution Information