Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Teaching with PMI

Valued Contributor
Valued Contributor

Hello, 

 

I have teached my one features with PMI's in a new MKE-Library. when I find the feature, 

the attributes dont show me PMI's with i have made with a Hole Callout and Champfer. 

All the other PMI's are found by NX, i also have named all the PMI's. 

 

Is that not working yet in NX 10 ? I would like to use the Hole callout for my thread because it selects all threads automaticly. 

 

Thank you 

NX 11.0.1.11
1 REPLY 1

Re: Feature Teaching with PMI

Siemens Phenom Siemens Phenom
Siemens Phenom

You can use symbolic thread annotation to define threaded hole or boss cylindrical faces.

 

Callouts are not supported.  Please see tdoc:

https://docs.plm.automation.siemens.com/tdoc/nx/11/nx_help#uid:xid1128418:index_mfgholemaking:id1456...

 

Reinier Capelle
NX CAM Development - Customer Success

Learn online





Solution Information