Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature based geometry set as floor or wall from rule

Experimenter
Experimenter

Hello All

Feature based machining and the MKE, do anyone know how to affect where the machining feature geometry is set for a volumbased facemill operation, how to get it set as floor instead as wall in the area object, continously I get it as wall but want the opposite

/Jonny 

1 REPLY

Re: Feature based geometry set as floor or wall from rule

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think that it is only possible to do so starting with NX 10, but could be NX 9 too.

 

OK found it in the NX 9 help under the topic CAM => Feature-based Machining => Teaching NX custom Features and Operations => Feature machining areas.

 

So best is to check the MKE customization tab if there are attributes Floor and Walls in the MILL_AREA geometry object.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information