Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature based machining-thread milling issue

Creator
Creator
Hi, I want to create a program for drill and thread mill strategy for similar features using Feature based machining . It has to be machined on 4-Axis Horizontal mill. Machining sequence: Step 1 : at B0 , drill dia 54.5mm till depth 75mm Step 2 : at B180 , drill dia 63mm till depth 40mm Step 3 : At B0 , using cutter dia 42.75,thread mill to be done to get M60X5.5 Thread. Right hand Thread, thread start as shown in jpg attached. Thread milling to be done only for 73mm depth. thanks in advance.
10 REPLIES 10

Re: Feature based machining-thread milling issue

Siemens Phenom Siemens Phenom
Siemens Phenom

We can help you get started if you let us know which exact version of NX you are using.

 

Tom van 't Erve

NX CAM Development

Re: Feature based machining-thread milling issue

Creator
Creator
Hi Tom van't Erve, I am using NX version NX9.0.3.4

Re: Feature based machining-thread milling issue

Phenom
Phenom

Here is a file with operations as descibed.

 

in "Operation" -> "Feature Geometry" -> "Reverse Direction" will change the tool axis.

Re: Feature based machining-thread milling issue

Creator
Creator

Hi Tom,

attached is the sample file

Re: Feature based machining-thread milling issue

Creator
Creator
Thanks Agrivas !!

Re: Feature based machining-thread milling issue

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

We will soon introduce a new capability in NX10.0.3 MP4 and NX11.0 that we call Operation SET Teaching. It's available as a preview in NX10.0.3 MP2; which is what I have used to create the attached AVI.

 

The AVI shows how to add new custom specific machining rules to the MKE from NX without every having to use the MKE. The input is a regular set of manually defined operations (using tools that have a library reference) under a feature group.

 

The "Teach Operation Sets" command will bring up a new dialog which allows users to define application criteria and tool selection criteria. The application criteria are shown at ~20 seconds into the AVI (in this example, ftr.DIAMETER_1 >= 50 and ftr.DIAMETER_1 <= 70). This can be anything but is used to define when this set of operations should be used.

 

The tool selection criteria are shown per operation. The tool type is directly taken from NX but we want to link the tool dimensions to the size of the feature. At ~30 seconds, the AVI shows the tool selection conditions for the DRILLING_63.0 operation (the tool diameter has to match the feature diameter and the tool flutelength has to be larger than the depth of the feature's DEPTH_1.

 

We hope that this new mechanism will lower the barrier to entry for Feature Based Machining and will encourage more users to customize their own rules.

 

Stay tuned for more information on this exciting new capability.

 

Tom van 't Erve

NX CAM Development

Re: Feature based machining-thread milling issue

Valued Contributor
Valued Contributor

Tom, that looks magic! Any special license requirements to make that work? Hole machining/FBM just got a hole lot better.

 

Spoiler
Pun intended.

Re: Feature based machining-thread milling issue

Creator
Creator

Thanks Tom !!!

Re: Feature based machining-thread milling issue

Siemens Phenom Siemens Phenom
Siemens Phenom

The new "Teach Operation Sets..." command will NOT require a new license.

Like with every FBM customization you DO need the existing FBM_AUTHOR license to be able to save your changes (either using the MKE to do File ->Save, or for the existing Feature and Operation Teaching capabilities).

 

Tom van 't Erve

NX CAM Development

Learn online





Solution Information