Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Feed Rates - Engage/Retract don´t take 100%Cut

Genius
Genius

Hi all,

 

I have an operation with a library tool (ball mill). tool_machining_data.dat has no entry for this tool. Set machining data (based on part/tool material, method, ...) is not used either.

 

When opening the operations feeds & speeds dialog it looks like this:

 

FeedsNSpeeds.jpg

When checking the Engage and Retract values with the operations Object->Information, I always get 107 instead of the 763.92 that should be taken from the Cut feed rate.

 

The 107 value only disappears when I re-enter value in the corresponding field (e.g. Engage).

 

I would expect the Information window to display the same value as set in Cut for Engage.

 

Do I miss anything or is this an incident? I am not quite sure what I have here.

 

Thanks upfront!

Best wishes,
Joachim

In production NX 12.0.1.7 D2
In testing NX 12.0.1.7 MP4
2 REPLIES 2

Re: Feed Rates - Engage/Retract don´t take 100%Cut

If the feeds are being output correctly, then it's probably a problem with the Information listing.

Please log a call and we can look in to it.

Mark Rief
Retired Siemens

Re: Feed Rates - Engage/Retract don´t take 100%Cut

Genius
Genius
Hi Mark,

I thanks for your reply. will report to GTAC.
Best wishes,
Joachim

In production NX 12.0.1.7 D2
In testing NX 12.0.1.7 MP4

Learn online





Solution Information