Cancel
Showing results for 
Search instead for 
Did you mean: 

Feed errror when using G96

Experimenter
Experimenter

2019-04-02_12-26-47.jpg2019-04-02_12-22-17.jpg

Hello

We have an error as you can see on the picture.

 

When we using M4 instead of M1=04 it works fine.

We have used CSEPreProcessLine.

 

We have created the mch file from start and inclued Basic.ccf and Siemens840D.ccf.

 

Do anyone have any idea?

 

Thanks

Christer

 

 

 

2 REPLIES 2

Re: Feed errror when using G96

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Christer,

 

first, try to avoid using CSEPreprocessLine! You´ll get other problems, you wont have.

 

I don´t see a need to add the S1 and M1=4 to CSEPreprocessLine. 

Look into the Sim15 nc simulation sample there are examples how to implement a e.g. S1 and M1=4. 

 

Thomas

 

 

Re: Feed errror when using G96

Experimenter
Experimenter

Hello Thomas

 

It did work when I went trough Sim15.

 

Thanks!

 

/Christer

Learn online





Solution Information