Cancel
Showing results for 
Search instead for 
Did you mean: 

Feeds and Speeds issue of Machining Data Library

Genius
Genius

Hello Folks

 

I tried to use machining data library to set feeds and speeds.

I set feeds and speeds as seen below:

2.JPG

 

But the Retract and Cross Over rates are 100%Cut which is not Rapid as I set in the machining data library.

ONLY Approach and Departure do work as I set.

1.JPG

Thanks

 

2 REPLIES 2

Re: Feeds and Speeds issue of Machining Data Library

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

This is a known bug and should be fixed in NX1847.
Send it to GTAC and they will provide you with a new TCL file you have to add in the recourse directory.

Sven Voeten
Pre-sales NX CAM / Manufacturing Consultant
cards PLM Solutions

Re: Feeds and Speeds issue of Machining Data Library

Genius
Genius

Sven

 

Thanks for your note, I just sent emial to GTAC. But it may take some time for reply, could you send me that tcl file, please?

 

Thanks

Learn online





Solution Information