06-15-2016 05:37 PM
I'm having trouble creating a finishing operation for a very simple semi-sphere that I've created. I need it to be smooth and preferably not leave the part (have as few rapid non-cutting motions as possible). I've tried using ZLEVEL_PROFILE, which didn't let me ramp on the part, and Streamline, which brought up an error stating that I didn't have a full drive surface.
I've also tried a few other options, but to no avail. Is there any simple, spiral operation in NX that I can use or am I missing some sort of parameter on the options that I've already tried?
Solved! Go to Solution.
06-15-2016 08:24 PM
06-16-2016 07:41 AM
06-16-2016 07:42 AM