Cancel
Showing results for 
Search instead for 
Did you mean: 

Fixed contour with Cutcom 2D (G41,42)

Gears Phenom Gears Phenom
Gears Phenom

Hello to everyone,

 

it is possible to do this operation with 2D radius cutter compensation?

Customer wants to machine modeled thread and use cutter comp.

 

(I see only toggle for 3D contact data. It gives me G41,42 but I want path generated on surface.)

 

thank you

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
10 REPLIES 10

Re: Fixed contour with Cutcom 2D (G41,42)

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

For Fixed/Variable contour operations you can get cutter comp on the tool centerline (compensate the dirrerence in tool radius), by adding a UDE Cutter Compensation. You can not output the contact point (compensate the full tool radius)

Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: Fixed contour with Cutcom 2D (G41,42)

What is your application for 2D cutcom in surface contouring? It would only be accurate for planar cuts on vertical faces, and for that we would use zlevel.

 

Mark Rief
Retired Siemens

Re: Fixed contour with Cutcom 2D (G41,42)

Gears Phenom Gears Phenom
Gears Phenom

This is floow wall. It is good.

 

aaa.jpg

 

Application : machining the steep surfaces with fixed contour - to get same type of paths on the picture above with any tool type.

I agree with customer´s demand and I suggested to add 2d cutcom option beside the 3d cutcom in fixed contour.

Now it is ER.

 

(I remember on guy he made special operation for this.

For hole chamfer machining. Quite nice piece of job.)

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Fixed contour with Cutcom 2D (G41,42)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX 10.0.3 has cutter compensation with cylinder milling.

NX 11.0.1 has helical cut-pattern with the floor wall operation.

Would be good to know which NX release we have to deal with Smiley Wink

If you need a 2.5D tool path stay with 2.5D operations, which support 2D cutter compensation OOTB.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Fixed contour with Cutcom 2D (G41,42)

Gears Phenom Gears Phenom
Gears Phenom

As I said in first post - customer wants to use it with modeled thread.

Big modeled thread= any surface.

Doesnt matter if it is end mill or T cutter, or ball mill.

Or for example milling the cone with 2D cutcom+contact data. Not zlevel or cavity.Fixed contour.

Floor wall and cylinder milling wont help.

There is no other solution to genarate contact data + switch on 2D utter compensation (G41/42).

NX11, any NX.

There is an ER on it.

 

 

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Fixed contour with Cutcom 2D (G41,42)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Using the drive method "Curve/Point" will output "contact data", since the tools tip is driven by the curve.

An edge is also accepted as a curve, just if you didn't know.

Adding cutter compensation trough the UDE will turn it on and off.

You can also create a ready to use operation template with the UDEs applied, so the user just has to select the correct edge and generate the tool path.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Fixed contour with Cutcom 2D (G41,42)

Gears Phenom Gears Phenom
Gears Phenom

Curve point generates path on the tool center.

We want path on the part.Radius compensation. And not only with this method.

Also adding UDE doesnt automatically respect direction of the path G41/42.

 

Possibility is add UDE and use not radial compesation but "zero radius" tool in the machinetool.

But again UDE is not automatic.

 

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Fixed contour with Cutcom 2D (G41,42)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you need a solution now, then you need to accept a work-around.

If the ER is not of interest to many customers of Siemens, then you will have to wait for ages or even forever.

May be it is easier to create a custom operation to provide the function the user needs.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Fixed contour with Cutcom 2D (G41,42)

I think you want 2 things: 

1. 2D cutcom in a 3D path - you need to do that in the post.

2. Path at the contact instead of tool center - either use a near zero tool, or output contact data and do it in the post. 

Mark Rief
Retired Siemens

Learn online





Solution Information