Cancel
Showing results for 
Search instead for 
Did you mean: 

Floor Wall, Flow wall IPW

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,,

 

what are the difference between , Floor Wall, Flow wall IPW

2 REPLIES

Re: Floor Wall, Flow wall IPW

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello karthik6,

 

basically it is the same operation type, but presented in two different templates. In these two templates, the settings are different.

 

Floor Wall is using the containment Blank thickness, where you can define the Floor and Wall Blank Thickness individually:

2017-09-13 10_19_54-Cutting Parameters.png

 

Floor Wall IPW uses the In Progress Workpiece. Either the selected blank is used (if it is the first operation), or it will see what Rest Material is left from previous operations.

2017-09-13 10_19_18-NX 11 - Manufacturing - [NX1101_Demopart_Adaptive_Milling.prt (Modified) ].png

 

You can find these option in the cutting parameters under the tab Containment.

 

Cheers,

Alexander

 

 

Re: Floor Wall, Flow wall IPW

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks mate.Nice explanation

Learn online





Solution Information