Cancel
Showing results for 
Search instead for 
Did you mean: 

Floor and wall - radius wall machining incomplete

Gears Phenom Gears Phenom
Gears Phenom

hello,

can you help me with setting of this operation?

I get incorrect behaviour. Preview is not full so toolpath also.

It left unmachined material.

(or report to GTAC?)

fl.jpg

 

(ipw, overhang 100, floor extended to blank)

Thank you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #
3 REPLIES 3

Re: Floor and wall - radius wall machining incomplete

Phenom
Phenom

Mucked around with this for some time, can confirm the problem but can't make it go away. How about planar profile as a temporary fix?

 

/Harri

Re: Floor and wall - radius wall machining incomplete

Siemens Phenom Siemens Phenom
Siemens Phenom

In the Containment tab of the Cutting Parameters, set the Blank option to Thickness and set the Wall Blank Thickness to 0.2500.

Re: Floor and wall - radius wall machining incomplete

Gears Phenom Gears Phenom
Gears Phenom

@jkane1 Thanks, it works now.

So ipw option is not reliable in case of wall machining?

 

@hjoy

so then I dont see meaning of existing of this operation and its all options Smiley Sad

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information