Cancel
Showing results for 
Search instead for 
Did you mean: 

Flowcut multiple with ipw and lots of crashes

Phenom
Phenom
Can't post file... this is a mold-type 3-ax cleanup operation with multiple side steps and depths. If IPW containment is off there's no problem. However there's way too much cutting air. With IPW containment I get multiple rapid violations. Engage is set to smooth so I can't manually override heights. I've fiddled with pretty much everything but no luck. Any ideas?

Harri
4 REPLIES

Re: Flowcut multiple with ipw and lots of crashes

If you can't post the part, can you at least add a picture showing the part, blank, and cut area? 

Is collision checking on in Non-Cutting Moves?

Have you considered using reference tool instead of IPW?

Mark Rief
Retired Siemens

Re: Flowcut multiple with ipw and lots of crashes

Phenom
Phenom
Will post a pic tomorrow. I'll also try reference tool, does this include the benefit of not cutting air?

I experimented with collision checking, violating moves still there.

Re: Flowcut multiple with ipw and lots of crashes

Phenom
Phenom
I talked with local support, I may have misunderstood ipw here. Seems it's for containment, not avoidance as such. So using too few levels (sides or z) will cause crashing even with ipw (containment) on.

Re: Flowcut multiple with ipw and lots of crashes

Phenom
Phenom
Ended up roughing some more and using just two passes for the flowcut. Seems to work!

Learn online





Solution Information