Cancel
Showing results for 
Search instead for 
Did you mean: 

Force Postprocessor to output a PLANE SPATIAL

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

Is there any way to force a 3+2 postprocessor to output a PLANE SPATIAL?,  when the plane is only a C axis rotation so the tool axis remains normal to XY plane no PLANE SPATIAL is otuput.

 

When I have to turn the C axis then no PLANE SPATIAL is performed and I need to force the postprocesor outputs it.

 

Frank.

1 REPLY 1

Re: Force Postprocessor to output a PLANE SPATIAL

Gears Phenom Gears Phenom
Gears Phenom

hi

I am not familiar with using library posts but you have to find output of plane spatial.

Maybe in intial move/ first move is plane spatial block with condition - so take a look in this condition and invstigate when occurs "return 0" (no block output) and "return 1" (output block).

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information