Cancel
Showing results for 
Search instead for 
Did you mean: 

Force once G98

Valued Contributor
Valued Contributor

Trying to get the post in postbuilder to out put the G98 at the beginning drill cyce.The best ive been able to get is posting at every x and y in the drill cycle.Would i use the mom_force_once command in each of the drill cycles?

22 REPLIES

Re: Force once G98

Gears Phenom Gears Phenom
Gears Phenom

MOM_force once G_return

 

(G_return is the word/address of G98/99)

 

Dont forget to add this address to cycle.

 

There is 3 options of G_return.

G98/99 ,G98 and G99.

The first one has variable index of array -  AUTOMATIC/MANUAL G98/99 - system can choose.

Last two is AUTOMATIC - G98 and MANUAL- G99

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Force once G98

Valued Contributor
Valued Contributor

Do add this too the can cycle in post builder?

Re: Force once G98

Valued Contributor
Valued Contributor

drill_cycle.PNG

Re: Force once G98

Valued Contributor
Valued Contributor

This is the G81 canned cycles I have in Post Builder doesnt seem to work this way 

Re: Force once G98

Gears Phenom Gears Phenom
Gears Phenom

what is not working?

you can add G_return address to cycle

-you can add it in "common parameters" section

- or you can also unlock customizing each cycle in "common parameters" section and then you can put G_return directly in the cycles blocks.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Force once G98

Gears Phenom Gears Phenom
Gears Phenom

It does not seem apparent on the Post Builder dialog but you use the Retract-to option to add the G98/G99 to the cycle statement.  Do this in the Canned Cycles - Common Parameters so it is added to each cycle.  Be carefull with the canned cycles in Post Builder, once you customize a cycle you cannon turn off the customization and any edits made to the general parameters will need to also need to made to any customized cycles.

 

 

 

 

 

  • RETRACT-TO.JPG
John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Force once G98

Valued Contributor
Valued Contributor

CYCLE PARAMETERS.PNGCYCLE PARAMETERS_2.PNG

Re: Force once G98

Valued Contributor
Valued Contributor

Works but can i keep it from posting every line?

Re: Force once G98

Gears Phenom Gears Phenom
Gears Phenom

Make sure the G98/G99 is set to modal and is not forced.

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information