Cancel
Showing results for 
Search instead for 
Did you mean: 

G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

Have a few tweeks to get the post to where I need it the opening motion move has dropped the G00 in the line I went to the motion section of the post in post builder and tried forcing it without results .The line will read like this G90 X1.2 Y2.8 S1200 M03 need the G00 in the line.Secound thing is the G40 posts on a seperate line above the linear retract in the cut would like to move it into the line with the G01 X AND Y movement.   Thanks

9 REPLIES

Re: G00 RAPID IN FIRST MOVE

Gears Phenom Gears Phenom
Gears Phenom

G40 - if you dont want it on separete line - remove G40 from - machine control - cutcom off.

 

G00 - better will be to share your postprocessor to see it

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: G00 RAPID IN FIRST MOVE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

RE: G00

Probably it is coming out in an earlier line in the output for that operation, and (as G_motion is modal) the post doesn't think it is needed (as it is already output).

 

A couple possible solutions (pending seeing your post)

- if this is a block in the initial move event (or first move) (or most anywhere in "Program & Toolpath" tab --> "Program" tab, but NOT in "NC Data definitions" -> "Block" tab), you can try toggling the "Force output" switch on the word

a) edit the block

b) right click on the "G00" word -> select the "Force output" option -> word should now have a white block on it (although not the docs for this menu, you can see the white "force" blocks on all the words here: https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:id1456358)

 

- alternately, you can add a "MOM_force once G_motion" just before the line(s) where you need the G00

 

- there's other ways as well.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

%
:0001
G40 G17 G90
(**********************************)
(  TOOL NUMBER   1  )
( SPOT_DRILLING )
( TOOL:0.250_SPOTDRILL )
( DIAMETER:0.250 )
( TOOL NOSE RADIUS:0.125 )
(**********************************)
N10 G28 G00 G91 Z0.0 T01
N14 T00 M06
N18 G54
N22 G90 X.6625 Y.3825 S1528 M03
N26 G45 Z2. H01
N30 G81 X.6625 Y.3825 Z-.0199 R.1 F1.5
N34 X0.0 Y.765
N38 X-.6625 Y.3825
N42 Y-.3825
N46 X0.0 Y-.765
N50 X.6625 Y-.3825
N54 X.66 Y1.1432 Z-.975 R-.8551
N58 X-.66
N62 X-1.32 Y0.0
N66 X-.66 Y-1.1432
N70 X.66
N74 X1.32 Y0.0
N78 G80
(**********************************)
(  TOOL NUMBER   2  )
( DRILLING )
( TOOL:0.159_DRILL )
( DIAMETER:0.159 )
( TOOL NOSE RADIUS:0.000 )
(**********************************)
N82 G28 G00 G91 Z0.0 T02
N86 T01 M06
N90 G90 X0.0 Y.765 S2402 M03
N94 G45 Z2. H02
N98 G83 X0.0 Y.765 Z-.4278 R.1 F2.4 Q.0856
N102 X-.6625 Y.3825
N106 Y-.3825
N110 X0.0 Y-.765
N114 X.6625 Y-.3825
N118 Y.3825
N122 G80
(**********************************)
(  TOOL NUMBER   3  )
( DRILLING_1 )
( TOOL:0.221_DRILL )
( DIAMETER:0.221 )
( TOOL NOSE RADIUS:0.000 )
(**********************************)
N126 G28 G00 G91 Z0.0 T03
N130 T02 M06
N134 G90 X-.66 Y1.1432 S1728 M03
N138 G45 Z2. H03
N142 G83 X-.66 Y1.1432 Z-1.2415 R-.8551 F1.7 Q.0955
N146 X-1.32 Y0.0
N150 X-.66 Y-1.1432
N154 X.66
N158 X1.32 Y0.0
N162 X.66 Y1.1432
N166 G80
(**********************************)
(  TOOL NUMBER   5  )
( COUNTERSINKING )
( TOOL:0.375_90_DEG_COSINK )
( DIAMETER:0.500 )
( TOOL NOSE RADIUS:0.250 )
(**********************************)
N170 G28 G00 G91 Z0.0 T05
N174 T03 M06
N178 G90 X0.0 Y.765 S764 M03
N182 G45 Z2. H05
N186 G81 X0.0 Y.765 Z-.095 R.3205 F1.3
N190 X-.6625 Y.3825
N194 Y-.3825
N198 X0.0 Y-.765
N202 X.6625 Y-.3825
N206 Y.3825
N210 G80
N214 G28 G00 G91 Z0.0 T05
N218 T05 M06
N222 M30
ESTIMATED MACHINING TIME: HOURS: 0 MINUTES: 8

Re: G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

THIS IS THE POST WITH THE G00 ABSENT FROM THE FIRST RAPID MOVE

Re: G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

:0001
G40 G17 G90
(**********************************)
(  TOOL NUMBER   1  )
( HOLE_MILLING_COPY )
( TOOL:0.750_ENDMILL )
( DIAMETER:0.750 )
( TOOL NOSE RADIUS:0.000 )
(**********************************)
N10 G28 G00 G91 Z0.0 T01
N14 T00 M06
N18 G54
N22 G90 X0.0 Y0.0 S764 M03
N26 G45 Z2. H01
N30 Z-.625
N34 G41 G01 X.0589 Y.0486 F1.5 D01 M08
N38 G03 X0.0 Y.1764 I-.0589 J.0503
N42 X0.0 Y.1764 I0.0 J-.1763
N46 X-.0589 Y.0486 I0.0 J-.0775
N50 G40
N54 G01 X0.0 Y0.0
N58 G00 Z2.
N62 G28 G91 Z0.0 T01
N66 T01 M06
N70 M30
ESTIMATED MACHINING TIME: HOURS: 0 MINUTES: 2
%

Re: G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

EXAMPLE OF THE G40

Re: G00 RAPID IN FIRST MOVE

Gears Phenom Gears Phenom
Gears Phenom

You have the G00 on the G28 line.  On most machines this is not needed (G28 is a rapid move )  Remove the G00 from that line and see if the post outputs is on the first move.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

That worked for the G00

Re: G00 RAPID IN FIRST MOVE

Valued Contributor
Valued Contributor

looks like taking the G40 out of the motion worked as well thanks for your help

Learn online





Solution Information