Cancel
Showing results for 
Search instead for 
Did you mean: 

G02/G03 in X..Y..R.. instead of X..Y..I..J..

Creator
Creator

Hello all,

I chang X..Y...I...J... To X..Y..R ... But have some problem. It appear alot or Cycle on Toolpath. Please view detail on my videos 

(view in My Videos)

5 REPLIES 5

Re: G02/G03 in X..Y..R.. instead of X..Y..I..J..

Legend
Legend

Hello

It is not so easy to switch from IJK (Circle Center) to R (Radius).

First read the Controller Manual.

If you want to Output Circle with Radius than you must consider following conditions.

 

Arc angle < 180°  Radius is positive  +R

Arc angle > 180°  Radius is negative  -R

Arc == 360°  not possible.  You need to split the arc

Also some Controller does not support 180°

So you need here also a workaround.

 

If you use PostConfigurator you only need to switch

"Circular Move Always with IJK"  to off

 

Regards

 

Re: G02/G03 in X..Y..R.. instead of X..Y..I..J..

Creator
Creator

Dear my friend,
Please help me to switch detail :
How i can make "Circular Move Always with IJK" to off

I use Fanuc 15 M controller

Re: G02/G03 in X..Y..R.. instead of X..Y..I..J..

Legend
Legend
First you have to generate your Post with PostConfigurator.
As i see you are working with PostBuilder. This is not the same!!!!

Re: G02/G03 in X..Y..R.. instead of X..Y..I..J..

Creator
Creator

Dear my friend,
I try to do the same you tell, but not chang I,J,K to R

Please see on videos :

Re: G02/G03 in X..Y..R.. instead of X..Y..I..J..

Gears Phenom Gears Phenom
Gears Phenom

in Postbuilder just:

1.remove IJK,

2.add R

{you can force XY R}

3.switch full circle\quadrant - and test both settings and use working one.

 

I have no problem with this.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information