Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

G183 For OKUMA, CSE driver

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello, Thomas!

What you can advise, what will be best way to add drilling cycle G183 for OKUMA? Subroutine? New method? Or - may be I can use a same cycles from FANUC?

 

Thank you!

 

Yuri

4 REPLIES 4

Re: G183 For OKUMA, CSE driver

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Yuri,

 

I am not very familiar with OKUMA and FANUC cycles. Looking form CSE a good approach is always to have a subprogram for the cycle itself. If it is hard to get them and the cycle itself you can also 'program' you own subprogram. I would avoid to put all into a meta code, that is not easy to create and maintain.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: G183 For OKUMA, CSE driver

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

On Okuma mill-turns, they use G18x like fanuc G8x

I.e. a Okuma G183 is very similar to fanuc G83

I'm thinking a G183 macro in the macro area?

Although you would need to understand tool axis & some other differences

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: G183 For OKUMA, CSE driver

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thanks for all for answers!

G183 not defined by default in CSE-drivers files. And my first idea was just copy G83 subroutine from FANUC cse folder, add variables to my OKUMA mcf-file, but OKUMA parser not understand "#", in this case a lot of editions for subroutine.

I will try both ways - G183 as metacode and G183 as subroutine.

Yuri

Re: G183 For OKUMA, CSE driver

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would have thought if you define the "cycle drill deep" cycle G code to 183, then it would just do the same thing (call sub G183) as if it was defined as 83 (call subroutine G83)

But other than 1 brief foray into CSE, I've had to revert to VNC so I don't really know how CSE works & maybe I'm way off base here...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information