Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

G31

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello! 

This topic have not direct relation to NX, but now I working for MAZAK e1060 postprocessor with measuring cycles, later I will show some results.

But now I have one question-problem.

My measuring part - in G54 (56, 55 not so important). For measuring motion I translate and rotate this coordinate system to target point with G68.2  and use G31 (with G43, of course) for probing. Ok, probe make few ding-ding and I can use #5061, #5062, #5063 etc. The question is: this values is coordinates for which point? Probe tip? Ruby ball center? Bottom plane of spindle? Pivot point of head? And - in WHICH COORDINATE SYSTEM. I know - not in the rotated and translated G54.. 

 

Do you have any same expirience?  

5 REPLIES 5

Re: G31

Are you using the Renishaw software or just a G31 line? 

Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Re: G31

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Hi,

 

The values stored in the skip read variables (#5061, #5062, etc.) after a G31 move are relative to the pivot point of B-axis head in the active coordinate system (G54, G55 etc. + shift). I am not sure how G68.2 affects these coordinates as I have not done any testing with it.

 

/Erlend

Re: G31

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Thank you, esn! I have a same results after testing. In this case (when I measure bore or boss with B<>0) I need algorithm to calculate 3points circle radius and center. Now I can do it, tor 3 points from B-Head I can calc R and XcYcZc for center circle. Of course - I must to recalc it to unrotated BC CSYS. 

Thank you in any case!!

Re: G31

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I have new information from my Mazak friends and from users manual. #5161..#5116 return skip signal in rotated after g68.

I will check it.

Re: G31

Pioneer
Pioneer
Spoiler
 

 

I check it on MAZAK e1060, for G31 and G68.2, one moment, #5161 and #5162 return X and Y for probe tip, but #5163 return Z for pivot point B HEAD.

 

Learn online





Solution Information