Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: G68.2 with RPY option

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi Ivan,

It looks that the tool length is not correctly calculated!? Please check at first the calculation without any tool or tool length. compensation. This helps to isolate the problem.

On which position is $TOOL transformation in the transformation stack in Machine Configurator? It should be at the end of the stack. When $TOOL is not displayed please add it and put it on the end of the stack.

When it´s not the tool. Do you have initial values defined in the axis properties?

Thomas

Re: G68.2 with RPY option

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Thomas, 

 

Sorry but yesterday I could not answer you. 

 

I try to execute the simulation without tool and the result is the same. 

 

These are my transformation (image03.jpg). I add the "$TOOL" trasnformation but I haven´t got changes. 

 

I think tool length compensation is not the problem here.

 

Best regard 

Ivan

Highlighted

Re: G68.2 with RPY option

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

mh.... lets try to isolate to problem.

please check the following NC Code with your expectation:

1.)
G53 X0 Y0 Z0
G68.2 P1 Q123 X0.0 Y0.0 Z0.0 I0.0 J0. K0.0
G53.1
G53 X0 Y0 Z0
2.) 
G53 X0 Y0 Z0
G68.2 P1 Q123 X0.0 Y0.0 Z0.0 I0.0 J90. K0.0
G53.1
G53 X0 Y0 Z0
3.) 
Txx M6
G53 X0 Y0 Z0 H1
G68.2 P1 Q123 X0.0 Y0.0 Z0.0 I0.0 J90. K0.0
G53.1 G53 X0 Y0 Z0
G53 X0 Y0 Z0
4.)
Txx M6
G54 X0 Y0 Z0 H1
G68.2 P1 Q123 X0.0 Y0.0 Z0.0 I0.0 J90. K0.0
G53.1
G54 X0 Y0 Z0 H1

 

 

Thanks

Thomas

Re: G68.2 with RPY option

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Thomas, 

 

Thank you very much for your help. 

 

Finally I managed to implement my function to perform the G68.2 successfully just as I needed.

 

I have used the PLANE function of the TNC parser and I edited it to implement the G68.2 like a PLANE SPATIAL TURN.

 

It works like i expected for Head-Head machine and for Table-Table machine.

 

Best Regards

Ivan

Re: G68.2 with RPY option

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Ivan,

 

thanks for your feedback and great to hear that you could finish successully your project! 

 

To look into the PLANE implementation is just the right approach. In general it doesn´t matter if its a cycle800, G68.2/G53.1 or PLANE SPATIAl. The cse core functions behind and their use is always the same.

 

I will prepare some training data this and next year which adresses exactly this topic and I will publish it as TechTip here in the forum.

 

Thomas

 

 

Re: G68.2 with RPY option

Pioneer
Pioneer

waiting for your training data ??

Re: G68.2 with RPY option

Phenom
Phenom
He was mentioning his series of videos (I think) which were posted at the beginning of 2018. I assume you have watched them and need more.the "Advanced overview" probably is one that shows some considerations. https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX-Manufacturing/CSE-Simula...
NX12.02
Windows 10 Pro
ITC Inc.

Learn online





Solution Information