Cancel
Showing results for 
Search instead for 
Did you mean: 

G71 Lathe Roughing Cycle

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Gentlemen,

     How do I get the output I want?  Is it a programming issue or a post issue?  

 

N6(ROUGH-BORE-.171-ID)

T0222G54( 4200048 )

G99G97G40G18S150M03P11

G00Z.05M08

X.1174Y0.0

Y0.0Z-.0591

G50S2500

G96S150M03P11

G71U.004R.005(ROUGH TURN CYCLE)

G71P7Q8U-.003W.002F.002

N7G01X.181Z-.152 (MOVE G01 DOWN 1 LINE ALONG WITH THE Z-.152. THIS LINE SHOULD READ N7 G00 X.181)

G01 Z-.152

Z-.161

X.171

Z-.201

N8X.1094

M05P11

M09

M1

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


1 REPLY 1

Re: G71 Lathe Roughing Cycle

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Jeff -

You can do this in the post (I've done it) but I forget what I had to do.  I don't remember it being particularly difficult, however.

Work thru the logic - procs, block templates, etc.

 

One other thing - note that NX typically moves to the first cut depth, THEN sets up the G71 cycle.  The cycle assumes you are at the OD, and adds ANOTHER cut depth, so the first pass is twice as deep as you want.  Not sure if they fixed that yet, but you should be able to figure it out to get the right X values.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information