Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Generate Tool Path when inside parameters dialog box


@Christoph2 wrote:

Hello Mark

 

The customization with the Explorer Nodes is really good but I have just one matter. Because I can't find all

options from dialog box from cutting parameters and Non cutting parameters. (Eg. pre drill pint, smoothing and some more)

That meaning is i can't add this the main window and I need still the buttons for these boxes and I have everything double.

Is there a way where I can find all options that I can include in the main window??

 

Thank you in advance


All of the items in the Cutting and Non Cutting dialogs should be available as customizable items. Please log a PR with GTAC if you find some missing.

Mark Rief
Retired Siemens

Re: Generate Tool Path when inside parameters dialog box

Experimenter
Experimenter

Sorry but I don't see all items just some. But some important are missing. 

Is there a possibility that its hidden? Do you have an idea?

 

Sorry I don't have a GTAC account and can't make a PR.

 

 

NX 11.0.1 MP2

Learn online





Solution Information