Cancel
Showing results for 
Search instead for 
Did you mean: 

Generating 3D Tool Assembly

Legend
Legend
Hi all,

Does anyone know a way to generate a 3D tool assembly from a parametric tool? In my understanding the Export Tool Part command is considered to be used with existing 3D tool assemblies to export them along with a parametric tool.

Is there a way to start from the parametric tool getting the 3D tool assembly parts?
Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5
3 REPLIES 3

Re: Generating 3D Tool Assembly

Legend
Legend

try this:

create a new part, start manufacturing

create the tool, with shank and holder, if necessary.

turn on manufacturing preference 'Display Selected Objects' 

Cattura.PNG

select the tool in Machine Tool View of Operation Navigator, the tool is shown with tip on WCS origin.

select Wave Geometry Linker in Assemblies Toolbar (Assemblies Application must be On) 

select Type Body and turn off Associative

 

Cattura1.PNG

then select the bodies from the displayed tool and press OK

the bodies are copyed in the work part. You can  now [ modify the bodies if needed ] export the tool to library and turn on Export Tool Part File option to save the tool part to UGII_CAM_LIBRARY_TOOL_GRAPHICS_PATH.

hope it helps

ciao

luciano

 

 

 

 

Re: Generating 3D Tool Assembly

Begining in NX 10.0.2, in native mode, you can select a tool and right click > Object > Export Part. Each section ot the tool (flute, neck, shank, holder) is a solid within the exported part:

  tool_export_part.jpg

This replaces several tricks that users used to use (like the one above) or grabbing the temporary tool from the assembly navigator.

Mark Rief
Retired Siemens

Re: Generating 3D Tool Assembly

Legend
Legend
Hello Luciano, hello Mark,

Thanks for both of your inputs. With that information I can do something.

Best whishes,
Joachim
Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5

Learn online





Solution Information