Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Generating Surfaces using NX OPEN and C++

Pioneer
Pioneer

(reposted here: http://community.plm.automation.siemens.com/t5/NX-Programming-Customization/Generating-Surfaces-usin...

 

Hi! I am trying to generate my custom parametric surfaces like NURBS, Bezier patches, for my research in Manufacturing. To start with I am trying to write a code in C++, for plotting a line, using NX OPEN application wizard of Visual Studio9 and then running the .dll file in NX. I am stuck on the point, about what libraries/functions to use so that when the code runs in NX, I can get the display of a line and two points on the NX Open Interface. I am sure, if I can get a line, I can extend it to get curves and subsequently surfaces.

 

2 REPLIES

Re: Generating Surfaces using NX OPEN and C++

I would post this question in the Programming and Customization Forum

Mark Rief
Retired Siemens

Re: Generating Surfaces using NX OPEN and C++

Pioneer
Pioneer
Thanks for guiding me to the right place!

Learn online





Solution Information